1/23/2023 9:47 PM | |
Joined: 1/21/2023 Last visit: 1/24/2023 Posts: 1 Rating: (0) |
Hi I need to display counter value every 4 seconds and then reset it over and over again. I am wondering about whether reading value from counter by mathematic instruction (with set option last value when EN=0) and resetting the counter with the same impulse is safe. I attached simple project where it works but I'm afraid of getting zeros because reset counter will perform faster than reading value. AttachmentCircuit Diagram2.zip (585 Downloads) |
1/24/2023 9:39 AM | |
Joined: 2/22/2008 Last visit: 5/10/2024 Posts: 2698 Rating: (206) |
You also can use attached version, created from your version with some changes. Flag M1 is a one cycle delay for the counter reset, the pulse generator ist changed by an on-delay timer. Regards, Scorp AttachmentCircuit Diagram3.zip (712 Downloads) |
Follow us on