Industry Online Support
Technical Forum
11/13/2008 5:05 AM | |
Joined: 9/27/2006 Last visit: 5/7/2024 Posts: 12257 Rating: (2666) |
Hello SexDriver; I could suggest you look at a very recent post on the same subject. J_Bell has a number of excellent suggestions you could look at: /tf/WW/en/Posts/23301 Hope this helps, Daniel Chartier |
11/13/2008 6:31 AM | |
Joined: 5/31/2007 Last visit: 3/29/2024 Posts: 90 Rating: (2) |
Hi,my man: I had already built Open IE Communications successfully between CP343 and 315PN/DP by Wizard software download form website without any problems, and nowmy questionsare: 1.Can I use "S7 connection" in thiscase? 2.If I can use "S7 connection" to build communications, what's the point I have to watch out?
|
Last edited by: SexDriver at: 11/13/2008 6:36 AMLast edited by: SexDriver at: 11/13/2008 6:35 AMLast edited by: SexDriver at: 11/13/2008 6:33 AM |
|
11/14/2008 10:28 AM | |
Joined: 5/31/2007 Last visit: 3/29/2024 Posts: 90 Rating: (2) |
Hello, gentleman : My CP343-1EX20 is V1.3.9 (file Attachment)and : 1. I had built S7 connection by the mentioned configuration and used FB14(GET)/FB15(PUT) in CP343 Station, and thisway is communication OK ; in the opposite , I failed in using FB14( GET)/FB15(PUT) in 315-PN/DP station. 2. I failed in builtthe S7 connection using SFB12(BSEND)/SFB13(BRECV) in both stations. Is there anyonegiving me more information? Thank you. Confused Asia, SexDriver
AttachmentPIC.zip (126 Downloads) |
Last edited by: SexDriver at: 11/14/2008 10:30 AM |
|
11/14/2008 1:00 PM | |
Posts: 5822 Rating: (411)
|
Hello, well... I do not know... I have tried it here and it works great. Best regards J_Bell AttachmentS7_comm_new.zip (145 Downloads) |
Follow us on