11/7/2017 4:40 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Perfect, you need V14 for this project and please bear in mind that I'm taking you in an entirely different direction from the rest of the suggestions in this thread. Best to have quick look first look at the example program I uploaded and get a very quick idea what I'm suggesting may work for you before investing too much time in it. I'm suggesting multiplexing which is explained in details in this blog. To open the project I uploaded earlier you need TIA V14 or later (SP1) -Download and unzip the file. -Open TIA V14 and go to menu "Project" then scroll down and select "Retrieve". -Browse to the file you unzipped earlier "Multiplexing_Example.zap14" and follow the instructions. -After the project is loaded simulate PLC_1 with PLCSIM then simulate HMI_1. -There's only one screen (Home), click in the textbox "Tank number" and enter the number 1 and notice the object/fields on the right update then click in the text box again and enter the number 2 and notice the difference. -That will give you an idea if multiplexing will work for you. |
This contribution was helpful to2 thankful Users |
11/7/2017 9:10 AM | |
Posts: 32 Rating: (1) |
Hello Kal.A Thank you very very match. It is indeed what I was looking for. I tried to make it myself but I have some question. - How did you make your “Tanks_Indexed” in your HMI? If I put in my Address it just disappears. - In Your HMI you have that “tank_info_1”. What is it? And how did you make that? - And if I want use a memory of it. How do I do that? which one do I take? - Is there a way that if automatically saves everything that when you put the power of and on that all the data is still on there? Like you did whit 1 and 2. |
Last edited by: PMVisser at: 11/7/2017 9:20:21 AMLast edited by: PMVisser at: 11/7/2017 9:28:38 AMLast edited by: PMVisser at: 11/7/2017 9:58:45 AM |
|
This contribution was helpful to1 thankful Users |
11/7/2017 4:07 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Hi PMVisser, I won't be able to reply in detail till much later in the day due to lack of time but you can get most of the answers to your questions by reading this blog post and it includes screenshots of how to set up an index tag. If you still have questions after you read that page, let me know and I will answer them later. Cheers Kal |
12/8/2022 6:42 AM | |
Joined: 5/10/2012 Last visit: 10/24/2024 Posts: 7 Rating: (0) |
Hello, I prepare a sample project in Tia V15 in order to change HMI recipes from PLC. Main code is: HMI tags>Recipe Change_Trigger>Events>Value change SetDataRecordToPLC Recipe number/name: Recipe_1 Data record number/name: Recete_Recete Name String(Should be same with Recipe Data Record tag in Recipe view) Output status message: On Processing status (Output,optional): Recipe_Loading Status(integer 2:loading in progress 4:loading successful 12:Loading failed) Fatih, AttachmentChange_Recipe_from_PLC2eng_V15.zip (350 Downloads) |
Last edited by: fatihsun at: 12/08/2022 06:44:01Last edited by: fatihsun at: 12/08/2022 06:51:53 |
|
8/1/2024 4:36 AM | |
Joined: 3/8/2019 Last visit: 9/5/2024 Posts: 2 Rating: (0) |
Hi all! This post was extremely useful, I have a project that needed exactly this, so thank you everyone! |
Follow us on