8/31/2023 12:41 PM | |
Joined: 7/13/2023 Last visit: 8/31/2023 Posts: 1 Rating:
|
Dear, I am currently polling data from a circuit breaker 3WA. I would like to read the active energy import registers. I've seen that there is a modbus table available but I am a bit confused about what register corresponds to which value and how are they stored. The modbus table is available here :Modbus Table 3WA 1/ For example, for the values stored as floats FP32, what is the most significant register and the less significant ? I need that information to be able to read it correctly. 2/ In the modbus table, what is the difference between the "EA_L1_IMPORT" and the "EA_L1_IMPORT_FLOAT" ? Are these instantaneous values ? (see attached image1) 3/ The overall active energy import is stored in the "EA_SUM_IMPORT_FLOAT" register, is it correct ?
|
Last edited by: AAZ2023 at: 08/31/2023 13:06:02 |
|
9/26/2023 6:54 AM | |
Joined: 9/25/2012 Last visit: 7/30/2024 Posts: 39 Rating:
|
Hello, please open a Service Request if you get no answer here. www.siemens.com/support-request |
Follow us on