12/29/2023 7:30 AM | |
Joined: 2/15/2019 Last visit: 11/11/2024 Posts: 3 Rating: (0) |
"Hello everyone, I need help with the ET200SP AI card 4-wire connection. In the attached picture, you can see all four wires coming from the AI module, but I want to provide external 24V to the transmitter. In the second picture attached, I have connected the external 24V. Is this wiring correct, or do I need to make adjustments? Your assistance is appreciated. Thank you." MLFB no 6ES7134-6GF00-0AA1 AttachmentET200SP_AI_Wiring.zip (476 Downloads) |
12/29/2023 9:14 AM | |
Joined: 8/12/2021 Last visit: 11/14/2024 Posts: 332 Rating: (31) |
Hi! You can find how to connect this cardin his correspondent manual. |
If this Information really helps, you could use the Rate function |
|
Follow us on