工业业务领域支持中心
Technical Forum
6/24/2007 12:09 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi, Please look in the handbookS7 300, ET200M IEx/O Modulesfor further information about the HART-modules. The Data-Record interface is mentioned in the chapter 4.9 Data record interface,and to read out the normal values with their status, see chapter 4.9.7 User data interface - input area (read). I don't have any example.... There is also another handbook ET 200M HART analog modules where the data recoords are also described in chapter 7 Data record interface and user data with in chapter 7.2.4 HART communication records. When you want to use the channels then you have to use SFC58/59, with SFC58 you have to choose which record you want to read with SFC59 and so on. ForPCS7 are blocks that do that for you. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on