4/11/2023 2:52 PM | |
Joined: 11/28/2022 Last visit: 10/31/2024 Posts: 4 Rating: (0) |
Hi all, I'm confused about decentral peripherie in the S7-1500. In the S7-300 CPU's, it used to be true that:
But now for the S7-1500 CPU's, all IO is available in the process image. Link |
4/11/2023 4:18 PM | |
Joined: 9/21/2012 Last visit: 11/14/2024 Posts: 4199 Rating: (474) |
Even in 300/400, if you use DPRD_DAT, it executes with the normal program execution, so it's not updating just like it is in a 1500. The whole concept is a little different in 1500, since the whole I/O area is in the Process image, it's just enought to read and write the I/O. |
Follow us on