5/8/2024 6:54 PM | |
Joined: 7/12/2018 Last visit: 6/25/2024 Posts: 18 Rating:
|
Hello everyone, I've been trying to export some archive data to further analyse, following this procedure, however I'm not being able to go through with it. I'm running WinCC Professional v15.1 upd5 and SQL Server Management Studio v20.1. I am able to get until the point 4.8 of the procedure, after which either of the options reports this error Is it possible that there's a problem with the installation of the OLE DB Provider? These are the properties I fill for the data source. It is also highly possible that I am making a very basic mistake, but I can´t see what could it be. I'd appreciate any help on this matter Thanks in advance. Best regards, Gonzalo Attachment38132261__Application_Reverse_Osmosis_DOC_en.pdf (70 Downloads) |
Last edited by: gniski at: 05/08/2024 18:55:45Minor corrections Last edited by: Jen_Moderator at: 05/10/2024 07:12:13PDF attached from link. Best regards, |
|
5/10/2024 4:57 PM | |
Joined: 7/12/2018 Last visit: 6/25/2024 Posts: 18 Rating:
|
Well, turns out I didn´t really know what I was doing and that caused all these issues. I do have some open questions that I will try to explore, but if someone wants to chime in, it would be welcome:
I'm attaching a document that helped me with the syntax and the concepts so that they are easily accessible Cheerio! Attachmentwincc_copackcsharp_en.pdf (82 Downloads) |
Last edited by: gniski at: 05/10/2024 17:26:40Grammar Best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on