4/19/2023 12:35 PM | |
Joined: 4/19/2023 Last visit: 8/17/2023 Posts: 1 Rating:
|
Hello Expert In Existing system Profibus DP card (CP5613, PCI) is used in the PC to communicate with ET200M (IM153-1) and its working and in same network we are using S7-1200 Profibus Master to communicate with ET200M and we are unable to communicate if we disconnect the PC then S7-1200 PLC is communicating with ET 200M Need your expert advise to establishing two profibus DP master with slave using same network, if not possible then please suggest any alternate option Attached the network architecture for your quick reference AttachmentNetwork Architecture-Layout1.pdf (285 Downloads) |
Follow us on