12/1/2021 10:03 AM | |
Joined: 3/15/2019 Last visit: 3/11/2024 Posts: 2 Rating: (0) |
Hai Im also on a similar problem i use Mebay Controller and want to send the functionskeys from winccruntime to the controller by modbus rtu the Problem is the controller needs to be writen in two registers at same poll (Function code 16) Write multiple Registers In the first Register will the controller Password be writen in the second register the Key Code for the Chosen Mode (Stop, Manual, Auto, Start, Test on Load...) When you find a way to force wincc to write data by Function code 16, please inform me Regards from Austria Andy ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/01/2021 13:39:31New subject after splitting |
|
Follow us on