4/4/2024 2:54 PM | |
Joined: 5/6/2022 Last visit: 7/5/2024 Posts: 429 Rating:
|
Hi VladD, The limitation remains the same. Not so much because of WinCC but because of Windows itself. With Windows 10 a WinCC Server can operate up to 3 clients. For more clients, you have to use a Windows Server: "WinCC V8.0: General information and installation: Software requirements for installing WinCC" Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
3 thankful Users |
Follow us on