8/10/2024 9:47 AM | |
Joined: 3/10/2022 Last visit: 10/1/2024 Posts: 4 Rating: (0) |
Our current system architecture is based on MRP R1 redundancy established with S7 1517H and ET200SP R1 IM system. other IO devices includes SINAMICS G120 VFD and Scalance XC200 network switches we have 5 MRP domains. MRP ring1 - mrpdomain1- 1517H left CPU as MRP manager(Auto) MRP ring2- mrpdomain2- 1517H right CPU as MRP manager(Auto) MRP ring3, ring4, rin5- mrpdomain3, mrpdomain4, mrpdomain5- Scalance XF204 2BA DNA redundant Y switch with one Y switch configured as MRP manager and other as client all other IO devices are configured as client while compiling, the error pops out as in the attached picture "Scalance switch interface belongs to a ring structure without MRP settings" also I get to see MRP Instances in configuration of Scalance XC 200 switches. if a switch is in mrpdomain3 and configured as mrpdomain3 and client device in instance1. what should we configure in remaining instances thank you AttachmentNW Arch.Wo-Logo.pdf (377 Downloads) |
Last edited by: seeker_ at: 08/10/2024 09:53:33 |
|
Follow us on