5/22/2024 6:56 AM | |
Joined: 2/23/2022 Last visit: 6/7/2024 Posts: 1 Rating: (0) |
-------------- On the FS:07 IndOS is pre-installed on the eMMC and this is the first boot device. The Industrial OS needs to be configured and has no pre-configured IP address - see here for more information. To make it easy for you: Press and hold the USER Button directly with powering on the device --> the eMMc is skipped and it should boot from your SD card with Example Image. Then change the boot order in Example Image to boot from SD Card at first. To change the boot order for good: sudo fw_setenv boot_targets "usb0 usb1 usb2 mmc0 mmc1" Connect the UART cable
Hope this helps. |
5/23/2024 9:00 AM | |
Joined: 6/14/2019 Last visit: 6/14/2024 Posts: 21 Rating: (0) |
Hi, I understand that using this method can change the boot order from eMMC to the SD card. However, it seems like the v01.02.01 image is not bootable on FS:07 device. Could you please confirm if you have tried booting the old image on the FS:07? Thanks. |
Follow us on