3/6/2019 10:08 AM | |
Posts: 51 Rating: (0) |
I have attached a project that calculates the percentage of running time for a specific machine against the time it could of ran for. Every 8 hours the timers are reset manually via a key switch (I8) I would like to remove the element of manual reset and have it reset every 8 hours at a specific time that is linked to a clock. Is this possible? so it resets at 6am, 2pm, 10pm Any support would be greatly received Attachmentpercentagecalculator opr.zip (258 Downloads) |
Last edited by: GUY7ON at: 3/6/2019 10:09:44 AM |
|
3/6/2019 2:33 PM | |
Posts: 51 Rating: (0) |
Works a treat :) thank you |
This contribution was helpful to1 thankful Users |
3/7/2019 4:39 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hi, That is just what i'm looking to do, are you using the logo tde or the hmi in your jpeg upload |
3/8/2019 8:29 AM | |
Posts: 51 Rating: (0) |
Hi Didn't use the TDE I used the LOGO! 8 and and programmed the HMI via the TIA portal then connected the two together :) |
3/9/2019 4:18 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
The HMI seems to be a KTP400, right ? Regards, Scorp |
Follow us on