2/27/2024 2:24 PM | |
Joined: 2/21/2024 Last visit: 5/6/2024 Posts: 4 Rating: (0) |
Hello I would like to be able to communicate 64bits between 2 coupled locomotives, controlled by ET200SP. For the time being, communication is carried out via PROFIsafe, security level SIL3 PLe. I would like to find a means of communication that allows me to be able to change coupling by being able to re-establish communication automatically. I thought I could use a gateway on each locomotive so that the communication would be from bridge to bridge. The advantage would be, from what I have been able to understand, that the 2 gateways recognize each other and ensure the transfer of data between the 2 PLCs linked to them. Could you, if possible, find a gateway reference that can meet my expectations? Or offer me another alternative? Thank you very much! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/28/2024 07:43:38Text formatting optimized and new subject after splitting |
|
Follow us on