12/10/2022 5:51 PM | |
Joined: 4/15/2022 Last visit: 6/26/2024 Posts: 4 Rating: (0) |
Hello! I know this was a while ago but, how did you manage this problem? I have the same problem. I have changed my pg/pc interface to PLCSIM ETH. ADAPTER TCPIP already. I have also tried to change the IE_general ip adress to same ipadress as my static ip in PLCSIM ADV. Im getting very frustrated. I have also inactivated all my other networks such as Wifi and family controller while trying to connect scada with plcsim eth. Thanks in beforehand! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/12/2022 10:41:07New subject after splitting May the waves be with you |
|
12/13/2022 7:40 AM | |
Joined: 4/8/2021 Last visit: 6/17/2024 Posts: 638 Rating: (102) |
Hi sinuswavesurfer, As durius_l said, it is important to know if PLC SIM or PLC SIM Advanced is used as only PLC SIM Advanced allows to establish outside communication. Can you ping successfuly the SCADA from the PC where PLC Sim is installed? Have you check if your communication protocol is supported? https://support.industry.siemens.com/cs/ww/en/view/109798879/142793849355 I would also check if latest updates/hotfixes for your version of PLCSim are installed. Hope it helps. |
Best regards, |
|
This contribution was helpful to1 thankful Users |
12/13/2022 7:40 AM | |
Joined: 8/3/2009 Last visit: 7/19/2024 Posts: 13341 Rating: (1690) |
Hello sinuswavesurfer We need some more information about this topic. -> Which SCADA System do you use? -> which Version of Step7 or TIA Portal Do you use (PLC SIM)? -> PLC Sim or PLC Sim Adv? -> Is the SCADA located on another PC system as the PLC SIM or on the same installation? -> Screenshots of what you have tested so far. --> If you use a WinCC System as SCADA you can have a look at this FAQ: https://support.industry.siemens.com/cs/de/en/view/109748099 https://support.industry.siemens.com/cs/ww/en/view/88193789 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on