6/12/2020 4:30 PM | |
Posts: 8 Rating: (0) |
Hello, I have a problem the pupitre Siemens 6AV6643-0DD01-1AX1 THIS IS THE LINK https://www.cofiem.fr/fr/22749-siemens-6av6643-0dd01-1ax1.html?gclid=Cj0KCQjwz4z3BRCgARIsAES_OVdbUuKb6_nnqL0HDRwDOt8dj-gNKnZwPPtLEAPfv4YMyux8mdPi0N0aAqS6EALw_wcB the 24 Volt power is ok but the device screen does not display anything! The screen seems to light in green and the power seems to arrive to the screen device but nothing is displayed so we cannot use it. Where can the problem be? is the screen out of service? |
6/12/2020 4:32 PM | |
Joined: 2/5/2013 Last visit: 9/27/2024 Posts: 321 Rating: (74) |
Hi fdfdf723, Please attach actual Photos of HMI panel so that it will be helpful for forum members. Br, AmolG. |
Please rate it. |
|
6/12/2020 4:49 PM | |
Joined: 2/5/2013 Last visit: 9/27/2024 Posts: 321 Rating: (74) |
Hi dfdfdf723, It will be better if you attach an image so that we can understand well and give our conclusion about what to do next. Even you can search related 'Search in Online Support'.I hope you will find related topics if you have urgency. Thanks in advance. |
Please rate it. |
|
6/12/2020 7:11 PM | |
Joined: 2/5/2013 Last visit: 9/27/2024 Posts: 321 Rating: (74) |
Please send it for repair to the siemens service center. Do you have final commissioning backups? Please note that the product is phase-out. Link Please ask for final commissioning backups.In case if it is not repaired and the new same HMI is not available in stock. Then we need to download in a successor version after a project migration |
Last edited by: AmolG at: 06/12/2020 19:12:30Please rate it. |
|
6/12/2020 7:15 PM | |
Joined: 9/27/2006 Last visit: 9/27/2024 Posts: 12283 Rating: (2685) |
Hello df; As long as you have the screen open, I would suggest you look at the small fluorescent tube that should be located at the back of the screen, on the circuit board. The screen uses LCD TFT technology, which requires a source of light for the screen image to become visible. If the backlight is no longer working, the screen will appear blank, with no graphics or characters visible, even though LEDs or other signals work. The screen uses a CCFL tube as backlight source.. Unfortunately, I cannot locate a part number for this CCFL tube in Siemens site, the screens have been declared obsolete for some time., However, when we were working with MultiPanels, we would source them from nearby vendors, such as this one: https://www.ccflwarehouse.com/ccfllamps.html The screenshot below has been extracted from this manual: https://public.eandm.com/Public_Docs/MP%20277_e.pdf Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/12/2020 19:26:55 |
|
This contribution was helpful to1 thankful Users |
9/25/2024 11:02 AM | |
Joined: 5/3/2023 Last visit: 9/25/2024 Posts: 5 Rating: (0) |
I had 2 displays LED went off, I could barely see the screen its like 0 brightness, I could not repair, just replaced. |
Follow us on