5/11/2020 11:50 AM | |
Joined: 4/28/2015 Last visit: 8/26/2024 Posts: 3345 Rating: (379)
|
Hi, the Example image is not an "example" of the SIMATIC Industrial OS. The Example (also based on Debian) is developed on github and you can use it for free. The SIMATIC Industrial OS is an official Siemens product which was running through system test. I wouldn't say that the Example image is less secure or reliable. And of course the Example Image can be installed on customers devices. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
6/13/2020 10:02 PM | |
Joined: 4/28/2015 Last visit: 8/17/2024 Posts: 37 Rating: (1) |
Hello, I purchased and have in hand 2 2050 0BA00 1YA2. How do I get the Simatic Industrial OS? Thanks D |
Follow us on