3/24/2023 8:12 AM | |
Joined: 11/8/2011 Last visit: 5/22/2024 Posts: 10 Rating: (0) |
Good morning, Yesterday the Simotion went to STOP. I connected and I see the warning 16#xxxx_4052on all my 10 winder station. I power off and on and turn it to RUN. As soon I make a work or slow speed the Simotion went to STOP again. After some tentative the only way to start the machine was to switch in Diam_mode_ext and then go back to Diam Calc Integral. I am using Interpolation_2. I am using LCON library v2.2.7 and the simotion is D455. Is there a problem of initialization of variables in the library when there is this warning? Thank you AttachmentFBWinderError.zip (405 Downloads) |
Follow us on