4/10/2024 6:50 PM | |
Joined: 10/2/2021 Last visit: 4/26/2024 Posts: 6 Rating:
|
Hello, I am trying to perform an safety integrated acceptance test for a G120C CU250S-2DP but in the end I always get an error message Error 3555:000003 with no suggestion about what may be the issue. The backup program is attached. I can run the commissioning wizard and motor automatic measurements without any problems. I enabled the extended safety functions to select SS1 (SBR) for the F-DI1 and deselected the rest. I am able to start and run the acceptance test! I can see the trace with the speed curves, SS1 and STO activation but when I press the "Next" button to finish the test, I get the error message. I have already tried many different setups for the monitoring time and Ramp-Down time for OFF3, but the result was the same. Thanks AttachmentHDGL - VFD_Migration.zip (65 Downloads) |
4/11/2024 7:57 AM | |
Joined: 6/27/2017 Last visit: 6/26/2024 Posts: 158 Rating:
|
Hi gnazareth, |
Follow us on