3/4/2024 1:03 PM | |
Joined: 12/14/2011 Last visit: 7/10/2024 Posts: 166 Rating:
|
Hi to all, i have the same problem in one of six G120C. Firmware version is 47.15.221. i am using profisafe. See the picture.
------------------------------------------------------------------------------------------ |
Last edited by: gigi_plc at: 03/04/2024 13:47:17Last edited by: The Helping Hand at: 03/07/2024 13:28:24New subject after splitting |
|
3/6/2024 4:14 PM | |
Joined: 12/14/2011 Last visit: 7/10/2024 Posts: 166 Rating:
|
Hi to all, here my firmware version. Many thanks. |
3/9/2024 9:31 AM | |
Joined: 9/21/2012 Last visit: 7/19/2024 Posts: 4023 Rating:
|
That is not the latest firmware available. The version you have is 4.7 SP13 HF4 [V04.71.52.21].You can update the drive firmware to 4.7 SP13 HF7, without the need to upgrade the device firmware in the PLC project. V4.7 SP13 HF7 [V04.71.52.28] SINAMICS firmware version 4.7 SP13 HF7 for SINAMICS G120C Download the latest firmware and update it to the drive. Lates one is V4.7 SP14 HF2 [V04.71.68.03]. |
Last edited by: Hati at: 03/09/2024 09:33:26Last edited by: Hati at: 03/09/2024 09:34:03Last edited by: The Helping Hand at: 03/11/2024 13:09:41Links optimized |
|
Follow us on