4/3/2024 9:09 AM | |
Joined: 12/23/2023 Last visit: 4/10/2024 Posts: 1 Rating:
|
Dear friends, Would you be so kind to tell me anything about how to measure this communication load? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/04/2024 05:59:12New subject after splitting. |
|
4/4/2024 6:18 AM | |
Joined: 1/21/2013 Last visit: 8/19/2024 Posts: 3044 Rating:
|
Hi Anders1993, To measure communication load, you need some additional equipment. This can be a network tap that mirrors all the data to a monitoring port to which you can connect your computer and capture all the data using, for example, Wireshark. There are also some companies that offer special devices for PROFINET monitoring. These allow continuous monitoring of your PROFINET installation and report any anomalies. You can also use a managed SCALANCE switch from the 200 family. These also allow you to configure a port as a monitoring port. Siemens offers SINETPLAN, the Siemens Network Planner. This tool is useful for simulating the network load on a configured network in the planning phase. However, it also allows you to import captures for a more detailed simulation. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on