7/19/2017 5:21 AM | |
Posts: 5 Rating: (0) |
I have a LOGO 8! FS4 LOGO SOFT 8.1v y SIMATIC S7 1200 1214 AC / DC / RLY with firmware 4.2 TIA PORTAL 14V. I try to connect but nothing happens, S7 not receive anything . the communication doesn't work. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/19/2017 8:23:33 AMNew subject after splitting |
|
5/31/2018 2:00 PM | |
Posts: 6 Rating: (1) |
I just did the same exercise, and It doesn't work. Like you I have a LOGO FS4 and 1200 V4.1. Please, we need a solution! |
6/4/2018 11:20 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by frantam is split to a separate thread with the subject Data writting from S7-1200 to logo NOT work. Best regards |
6/18/2018 9:17 PM | |
Joined: 12/18/2014 Last visit: 11/4/2024 Posts: 34135 Rating: (4253)
|
Create the connection with the LOGO! as a client and the S7 as a server. In TIA: AttachmentScreenshots.zip (617 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on