4/1/2017 6:24 PM | |
Posts: 9 Rating:
|
Just to Hijack this thread a little Got an AM2 AQ myself using two analog outputs 0-10v to control a device Checked the Manuel page 48 :) so one uses V1 and M1 ,other uses V2 and M2 voltages work great in 0-10V range with appropriate software no problem. The issue I have is the device uses a stereo Aux cable which only has three connections. The voltages work fine on V1 and V2 if I use M1 or M2 so which do I use ? does it matter ? or should I connect M1 and M2 together then use that as a conman return feed? Sorry for not being very technical but using the Logo8 to control something in my hobby and no electricain here just a *** Many thanks for any replies Zeus ------------------------------------------------------------------------------------------ |
Last edited by: ZeusT32 at: 4/1/2017 6:25:07 PMLast edited by: Min_Moderator at: 4/3/2017 10:48:26 AMNew subject after splitting |
|
4/4/2017 1:38 PM | |
Posts: 9 Rating:
|
Thanks worked a treat |
Follow us on