5/13/2021 5:40 PM | |
Joined: 12/18/2014 Last visit: 8/22/2024 Posts: 33603 Rating:
|
Good luck ... |
This contribution was helpful to
1 thankful Users |
5/19/2021 8:17 AM | |
Joined: 4/28/2021 Last visit: 6/27/2022 Posts: 32 Rating:
|
Hello everybody. I tested the program and it works medium. The laser can read the distance, i can also count up/down on the TD. The engine goes left and right. But the stepper motor nevers stops on the exact position. When it almost reaches his point he goes left, then right, again left and so on. i'm talking about 5-8cm too much to the left, and 5-8cm too much to the right. What do i have to change to the program? Attachmentcount scale laser sensor up down stepper motor.zip (362 Downloads) |
5/19/2021 8:57 AM | |
Joined: 12/18/2014 Last visit: 8/22/2024 Posts: 33603 Rating:
|
Try it with other settings in the ON-OFF parameters of the analog comparators, e.g. with 5. |
Follow us on