5/21/2021 3:13 PM | |
Joined: 4/28/2021 Last visit: 6/27/2022 Posts: 32 Rating:
|
Okay, can you help me with what that i have to change? |
5/21/2021 3:22 PM | |
Joined: 4/28/2021 Last visit: 6/27/2022 Posts: 32 Rating:
|
Yes, i think that will be a good solution. |
5/21/2021 3:32 PM | |
Joined: 4/28/2021 Last visit: 6/27/2022 Posts: 32 Rating:
|
yes, perfect thank you! |
This contribution was helpful to
1 thankful Users |
5/21/2021 3:34 PM | |
Joined: 12/18/2014 Last visit: 8/22/2024 Posts: 33603 Rating:
|
Okay. |
5/21/2021 4:05 PM | |
Joined: 12/18/2014 Last visit: 8/22/2024 Posts: 33603 Rating:
|
Here is the program. But please note: The slide will never stop to the nearest millimeter.
Attachmentcount scale laser sensor up down stepper motor_V2.zip (338 Downloads) |
This contribution was helpful to
1 thankful Users |
5/25/2021 3:59 PM | |
Joined: 4/28/2021 Last visit: 6/27/2022 Posts: 32 Rating:
|
Okay I tried it, it works almost good. It goes indeed just in 1 direction. But I still have a pretty big meaurement range. 40mm maximum to the left and 40 mm maximum to the right . (40 + 40 =80 mm range) Sometimes it is just 4mm but sometimes it is 35mm to much. With the on - off settings 45-35. How can I change that, or how do i have to set the on-off settings of the analog comporator? Attachmentprogram F3.zip (319 Downloads) |
Follow us on