2/8/2015 10:30 PM | |
Posts: 15 Rating:
|
I've set up a logo with 4 modules am2 rtd and did not work either, I configured the logo 8 0 AI, physical position is logo8 below a digital input / ouput and after the 4 modules am2 rtd, I can transfer the program but with the online test, the analog inputs do not change, even I have proven with one module and does not work references of the modules are digital input / ouput 6ed1-055-1mb00-0ba2 am2 rtd 6ed1-055-1md00-0ba2 the probe is 2 wires U1 and 1v1 is a bridge between ic1 and u1 + I put the pt100 where is the error Attachmenttest AM2 RTD.rar (235 Downloads) |
2/9/2015 6:33 AM | |
Joined: 12/18/2014 Last visit: 7/21/2024 Posts: 33382 Rating:
|
The Bridge must between Ux- and ICx, one wire on Ux- and the other on Ux+. None of the 8 channels brings a value? |
Follow us on