11/26/2015 11:30 AM | |
Posts: 3 Rating:
|
New to Logo! Have bought a starter kit with Logo8 and TDE. I have set an ip-address on TDE and can ping it. But I cant get in contact with the Logo8. All I know is the MAC-address. How do I set the ip-address? If it has an ip-address, which I dont know, can I reset it? Or how do I get in contact with it from my PC. I only have ethernet cable. Thank you :-) ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/27/2015 9:22:28 AMNew subject after splitting |
|
11/26/2015 11:44 AM | |
Joined: 12/18/2014 Last visit: 7/19/2024 Posts: 33376 Rating:
|
Select in the main menu of TDE "LOGO! Selection", press OK button. Then enter the IP address of the logo. |
11/26/2015 12:47 PM | |
Posts: 3 Rating:
|
So you mean that I put in the ip-address that I want the Logo to have? I have tried, does'nt work :-( |
Follow us on