11/1/2016 9:15 AM | |
Posts: 3 Rating: (0) |
Hello bergmanu, is there a manual how to build the image for an IoT2040 or is there a download link for an example image? I downloaded the example image for IoT2000 and wrote the image to a SD card. I was not able to connect through eth0 interface (IP 192.168.200.1). After using the FTDI cable following boot error was shown:
May be this image is not suitable for an IoT2040? Is the device tree configured wrong? Can you please help on this issue? ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_7366268 at: 11/1/2016 9:46:20 AMLast edited by: The Helping Hand at: 11/2/2016 2:40:43 PMNew subject after splitting |
|
11/2/2016 7:56 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hello Mustafa, the image provided is suitable for both, IOT2020 and 2040. It seems that you are using prototype hardware. Please refer to "Cannot connect to 192.168.200.1". Best regards! |
Last edited by: bergmanu at: 11/2/2016 7:57:09 AMNot working for IOT2050 support anymore from March 1st, 2024. |
|
11/3/2016 5:55 AM | |
Posts: 3 Rating: (0) |
Thanks for your support. |
Follow us on