4/6/2024 8:04 PM | |
Joined: 6/23/2023 Last visit: 5/16/2024 Posts: 1 Rating:
|
I'm using a 1214-DC/DC/DC CPU with the IP set as 192.168.100.10, in the pictures is possible to see that I establish the network with the device and are occur the exchange of packages but when I do a requsition of packages for my device I don't receive nothing, even when I do some mistake in the configuration of the requsition I receive the code #8200 that show some inconsistence. The device is a Gefran GFX4 Controller, this contoller have the IP Address set as 192.168.100.12 the modbus address is set as 20, using the Gefran Software I can find and read some data from teh controller, using any other modbus scanner in the computer I can't read nothing I don't kow If I'm make some mistake in the data requisition or is a Bug that shows that the packages are received by CPU but nothing are received. Anybody have Idea, what happen in this application? Best regards Attachmentmodbus.zip (123 Downloads) |
Follow us on