3/28/2014 5:23 PM | |
Joined: 8/16/2010 Last visit: 10/30/2024 Posts: 638 Rating: (12) |
Yes I have pressure sensor...Which goes to Analog input... But I especially interested in code.... |
3/30/2014 4:04 PM | |
Joined: 8/16/2010 Last visit: 10/30/2024 Posts: 638 Rating: (12) |
thank's for help... I done code in s7-300 because i can simulate in plcsim... this version can only start pumps in defined conditions... Now, I need suggestion, is this good code? Is that right thinking? How to do stop of pumps in automatic mode? That means to determine last running pump. How? If actual pressure greather than setup pressure turn off last running pump.. AttachmentPumps.zip (288 Downloads) |
Last edited by: Milosh at: 3/30/2014 4:08 PM |
|
4/5/2014 9:48 PM | |
Joined: 9/1/2005 Last visit: 10/25/2024 Posts: 4109 Rating: (195) |
follow up question published by karthikkis split to a seperate thread with the subject Need help in LAD - System with 4 pumps. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
4/8/2014 11:08 AM | |
Joined: 1/5/2011 Last visit: 6/15/2024 Posts: 815 Rating: (123) |
Hi Milosh, since I'mpracticing my SCL a bit, I've tried to create your project (or at least something similar since I couldn't understand your requirements completely). See attachment, I added comments to make it a bit understandable. I hope this helps. (I tried to upload the program in *.rar but that is not possible, so I had to convert is to a pdf) Kind Regards, Jens AttachmentPumpSelection1.pdf (272 Downloads) |
Keep it simple and on-topic. |
|
Follow us on