2/15/2017 4:48 PM | |
Joined: 12/18/2014 Last visit: 8/25/2024 Posts: 33614 Rating:
|
There are two different hardware versions of the LOGO! 0BA8. The older one is 0BA8.Standard. It has the Fimverwareversionen V1.08.01 to V1.08.03 (corresponds to the production stands FS01 to FS03). With the LOGO! Soft Comfort V8.0.x, only programs for the 0BA8.Standard can be created and edited, but not for the 0BA8! .FS4. For the correct upgrading also the V8.1 please see this topic: Upgrading from LSC V8.0 to LSC V8.1 Edit: For upgrading start the LSC V8 as an Administrator. |
Last edited by: ixo65 at: 2/15/2017 4:49:59 PM |
|
This contribution was helpful to
1 thankful Users |
2/15/2017 4:55 PM | |
Posts: 158 Rating:
|
I re-opened as administrator and it loaded....THANK YOU |
Last edited by: markheuer at: 2/15/2017 4:57:59 PM |
|
This contribution was helpful to
1 thankful Users |
2/15/2017 5:02 PM | |
Joined: 12/18/2014 Last visit: 8/25/2024 Posts: 33614 Rating:
|
I also updated many times, and I never had a problem. Also not with the upgrading fom V8.0 to V8.1. There you can go another way: Download from this Siemens Website Demo software , upgrades/updates, Drivers the upgrade-file, it is a "Setup.exe" file. After downloading run the Setup.exe as an Administrator. |
7/26/2017 8:11 AM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating:
|
New question published by gustavosa is split to a separate thread with the subject Is it possible to create a file in a SD card to load into old version firmware v1.08.03 with LSC 8.1 and new LOGO?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on