4/13/2016 11:31 AM | |
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating: (42) |
Find the screenshots... |
6/27/2016 10:40 AM | |
Joined: 10/7/2015 Last visit: 3/20/2024 Posts: 56 Rating: (50) |
Hi all, pls check if the LoadPicture Script when putting a file into the navigator via drag and drop it will be copied here - this is a physical location INSIDE of a working layer folder structure COMOSPT\WO00002\aa\ABC12DEF.jpg in object debugger it looks like this ( a.fullfilename \\servername\share\Comosdoc\COMOSPT\WO00006\aa\ABC12DEF.jpg that is a valid (but working layer fixed) path that can be put into the loadpicuture script Set p=LoadPicture("\\servername\share\Comosdoc\COMOSPT\WO00002\aa\ABC12DEF.jpg") set picture = p That doesn't match the script any more. It is better to put icons and symbols into folders being independent from working layer mechanism, example SO1\Icons\MyIcon001.jpg This path will always be valid. |
Last edited by: Einhörni at: 6/27/2016 10:46:23 AM |
|
Follow us on