5/7/2024 6:30 AM | |
Joined: 11/22/2016 Last visit: 6/14/2024 Posts: 2 Rating:
|
I have a Scalance W761-1 as a client, to this W761 I have a S7-1510SP PLC connected. The W761 is connected to our WIFI network. I have the strangest behavour. When I start the machine (battery operated AGV) I can ping the W761 from my computer by WIFI. I can connect to the W761 user interface by WIFI and initilize a ping from the W761 to the PLC. It works. But I cant ping from my computer to the PLC directly. I can't go online with TIA portal, the PLC isn't reachable. But if I connect to the PLC with a network cable and then goes online, it works. Then I disconnect the cable and tries again to go online by WIFI, then it works. And then it works until I restart the AGV. I can't figure out why. W761 as Client Attachmentconfigpack_SCALANCE_W700.zip (62 Downloads) |
Last edited by: AutoGen_4866583 at: 05/07/2024 06:31:35 |
|
Follow us on