7/29/2023 8:50 PM | |
Joined: 10/15/2022 Last visit: 8/15/2024 Posts: 66 Rating:
|
Hi, LOGO! enthusiasts. The "Proportion Calculation Demo" program is designed to calculate the final result depending on the value of the first sensor, the reduction effect % and the value of the second sensor. This function can be used, for example, to control an outdoor fountain, taking into account the effect of the wind. In case of strong wind, some of the erupting water is blown away. Therefore, the water bath of the fountain must be filled with new water more often. One way to reduce water loss is to reduce the performance of the variable frequency drive that drives the pump. Therefore, the water level is also lower and the wind "carries" less water away. The zip file contains the program, diagram and description (3 files). Tested on LOGO!8 6ED1052-1MD08-0BA1 (with firmware 1.83.02). Andrus AttachmentProportion calculation demo.zip (379 Downloads) |
Last edited by: Andrus_Saar at: 07/29/2023 20:52:55Last edited by: Andrus_Saar at: 07/29/2023 20:56:05Last edited by: Jen_Moderator at: 07/31/2023 10:53:53Text formatting optimized. Last edited by: Andrus_Saar at: 08/08/2023 16:45:13Last edited by: Andrus_Saar at: 08/08/2023 16:47:52 |
|
This contribution was helpful to
1 thankful Users |
Follow us on