5/12/2015 10:34 PM | |
Posts: 10 Rating: (0) |
So it should be connected like on the attached image ? |
5/12/2015 10:34 PM | |
Posts: 10 Rating: (0) |
So it should be connected like on the attached image ? |
5/13/2015 5:45 AM | |
Joined: 12/18/2014 Last visit: 7/21/2024 Posts: 33382 Rating: (4143) |
Yes, correctly. |
This contribution was helpful to1 thankful Users |
5/14/2015 8:11 PM | |
Posts: 10 Rating: (0) |
...and finally if I have multiple outputs with coils etc. can I connect just like that: |
5/14/2015 8:53 PM | |
Joined: 12/18/2014 Last visit: 7/21/2024 Posts: 33382 Rating: (4143) |
The wiring is okay. But have you considered that the transistor outputs can only supply 0.3 amps? |
5/17/2015 11:06 PM | |
Joined: 12/13/2014 Last visit: 7/20/2024 Posts: 144 Rating: (12) |
DM24, probably all other LOGO!-s with transistor output used Infineon ITS4140 power switch per channel. According to datasheet freewheeling diode is already present. |
Follow us on