9/28/2015 2:21 PM | |
Joined: 7/19/2011 Last visit: 7/16/2024 Posts: 262 Rating: (5) |
Dear All How i can read a double word in 30000 series address in modbus communication in TIA V13 advance Runtime. Actually i am communicating with a Energy meter on Modicon Modbus RTU protolcol in TIA V13 advance. There are addresses in 30000 series .i.e. input registers. Now my issue is that the address which required single word length is communicating but those who required 2 word are not communicating. Kindly tell how i can use 2 words length in Input register series. Kindly check attachment for energy meter manual for reference. ------------------------------------------------------------------------------------------ AttachmentL&T Vega Multifunction meter.pdf (283 Downloads) |
Last edited by: Min_Moderator at: 9/28/2015 4:28:53 PMNew subject after splitting JAVED AKHTAR |
|
9/29/2015 2:34 PM | |
Joined: 1/17/2007 Last visit: 7/16/2024 Posts: 1543 Rating: (534)
|
What do you by "not communicating" exactly?
I also noted that some values are sent as 3 registers (48-bits). I have never, ever seen this before and I have no idea hoe they have been encoded as the manual fails to mention it. |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
This contribution was helpful to2 thankful Users |
10/17/2016 5:43 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by Ryan_Ryan is split to a separate thread with the subject Modbus, access only first 10 coils of slave compressors. Best regards |
10/2/2017 9:05 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
New question published by Mahesh_Renuse is split to a separate thread with the subject How to use Modicon Modbus RTU Driver & connection details?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on