4/4/2022 3:19 PM | |
Joined: 3/9/2018 Last visit: 7/18/2024 Posts: 188 Rating: (14) |
U can try use as second NPort5130 in a master slave setup (RS485 - LAN - RS485), but I have no experience with this. In theory this should work. Are you not able to communicate to the OPC server om the LAN port of the cMT-G02 and use the RS485 port on the PLC? This is a way to "communicate over LAN" (ISO-TSAP on port 102), or i'm still missing something. The Communication processor CP 243-1 Ethernet adapter. Any LAN MPI Gateway should work. but because the cMT-G02 is a LAN gateway it makes no sens to me for you to acquire a CP 241 or an additional LAN gateway. |
Follow us on