1/30/2024 1:23 PM | |
Joined: 5/12/2006 Last visit: 6/14/2024 Posts: 22263 Rating: (2990)
|
please add screenshots how the device is displayed exactly in scout |
1/31/2024 12:03 PM | |
Joined: 3/13/2019 Last visit: 6/2/2024 Posts: 152 Rating: (2) |
Here I am attaching img of scout configuration software ,when I try to accessible nodes I can't accept devies in project.....Accept function shows disable Pls help me out of that Scout software version is V4.5 Regards, Pankaj Attachment1000090366.pdf (133 Downloads) |
2/1/2024 2:26 AM | |
Joined: 3/13/2019 Last visit: 6/2/2024 Posts: 152 Rating: (2) |
Dear sir , I have installed SSP_SINAMICS_G120_V4_7_SP13_HF3.zip (19,4 MB) but this is not compatible with scout V4.5. After that i checked in help installed devise then i found SSP for G120 240B-2 is already installed. Now why accessible devise is not showing ????? and accept button is disable. Here i am sharing installed devise in scout V4.5.... Regards, Pankaj Tiwari |
2/1/2024 12:04 PM | |
Joined: 3/13/2019 Last visit: 6/2/2024 Posts: 152 Rating: (2) |
Dear sir pls find control unit detail in attached img. |
2/1/2024 12:08 PM | |
Joined: 5/12/2006 Last visit: 6/14/2024 Posts: 22263 Rating: (2990)
|
for this G120 with this FW you need a newer Scout version |
This contribution was helpful to1 thankful Users |
Follow us on