7/6/2020 9:52 PM | |
Joined: 2/27/2014 Last visit: 8/28/2024 Posts: 14 Rating: (0) |
Hi I backed up the PLC and NCK data using pcin software. When I attempt to restore I get attached error during transfer. These are steps I used during restore on 810D ccu 3.4 software ver 6.4: Change access level to Manufacturer using sunrise password Goto Services--> set com port and baud rate--> select data in--> press start (At this point I would have already setup my pcin software send data) After i press start a dialogue box appears with the option of selecting "path/workpiece from archive" and below there is a message "no access rights". After clicking ok transfer will begin and then it will stop after few seconds with an error which I have attached. Please can someone assist me ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/07/2020 09:35:54New subject after splitting |
|
7/7/2020 9:51 PM | |
Joined: 2/27/2014 Last visit: 8/28/2024 Posts: 14 Rating: (0) |
Hi Profibus connection is working. That is correct I have 810D with PCU20. We had to change the battery due to “2100 NCK battery warning threshold reached” alarm. After changing the battery (we replaced the battery with a non siemens 3v battery) we still get " 2102 NCK battery alarm" In regards to the problem I posted earlier I managed to get the NC transfer process to START when I used pcin within windows xp 32-bit (VM). For some reason windows 7 64 bit was giving me a problem. The problem I have now is that I get the following error when restoring the NC "There is not enough memory to install an load-object". The total NC memory available is 1247 KB, 1017.277 KB is free after NC reset. I tried to increase the SRAM memory in the following location 18230 MM_USER_MEM_BUFFERED- I changed currently set value from 1247 to 1592 KB to match the size of the NC back up. But those changes are never saved. Are the changes not saved because of the battery alarm "2102"? Are there any other ways to increase the NC memory? Attachment810D.pdf (151 Downloads) |
7/8/2020 5:57 AM | |
Joined: 2/27/2014 Last visit: 8/28/2024 Posts: 14 Rating: (0) |
Hi. Thank you I will do so and let you how it goes. Do you have to install a siemens battery? |
Follow us on