8/11/2017 10:11 AM | |
Joined: 8/24/2016 Last visit: 6/30/2022 Posts: 56 Rating:
|
Hi i have reopend this post after 8 years for the same function of retrofitting.Even our system is equipped with MMC103 and needs to be fitted with PCU 50.3.Only thing that troubles me is the current system is using only custom made screens and no CNC programming code.Only thing i require right now is I need to transfer all those screens from my MMC103 to PCU 50.3.I dont know wheter it is a Wizard screen or not.But those screens are not developed with any external software coz i am able to see some coding related to the screen development but not able to catch them .So can anyone please tell me the way for transfer those custom screens from MMC103 to PUC 50.3.Thnx for everyone who r gonna reply to me in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/11/2017 2:11:52 PMNew subject after splitting |
|
8/14/2017 7:11 AM | |
Joined: 8/24/2016 Last visit: 6/30/2022 Posts: 56 Rating:
|
|
11/20/2019 1:45 PM | |
Joined: 12/3/2012 Last visit: 3/22/2022 Posts: 2 Rating:
|
Hi. Were you able to solve this issue? I'm facing an issue with a Deckel Maho machine I've purchased- the PCU50 unit is not OK and needs to be replaced. Having two machines of the same type, I've come to realise I would be happier with a newer PCU module than what is currently in the machine (6FC5210-0DF22-0AA0). The machine has customised screens. Were you able to upgrade your unit? Did you face any issues while migrating the screens? Best regards Jaideep
|
Follow us on