3/31/2015 7:04 AM | |
Posts: 2 Rating:
|
Hi, Please help to solve this PLC -PC communication issues . I have tried the following procedure to upload the program from the Siemens simatic ET 200 SP to the PC CPU model # 1512 SP – 1 PN 6ES7512 -1DK00-0AB0 , But when i connected the pc to PLC and tried to configure the connection – then it was showing the device type as S7 1500 CPU .
Procedure / Steps used to upload the Program from PLC To PC
1 . Created new project.. 2. Configure device option. 3. add a new device option . 4. Tried to add CPU – Unspecified CPU 1500 . 5 . Also tried the CPU – Unspecified simatic ET 200 SP. 6. Tried Detect configuration of the connected device option.
But during the detect configuration procedure . it was showing an error message of 0 compatible devices of 1 Accessible device found . In this way i was not able detect the PLC using TIA Portal V13 Also the PLC was showing Error Indication ( Red LED flashing ) , When i tried the upload option from the menu. . Please provide us your valuable Instructions to Upload the program to the PC / solve this PLC – PC communication issues /
---------------------------------------------------------------------------------------------------- |
Last edited by: tinto at: 3/31/2015 7:05:45 AMLast edited by: Min_Moderator at: 3/31/2015 3:14:30 PMNew subject after splitting |
|
3/31/2015 3:18 PM | |
Posts: 46 Rating:
|
Hi tinto, I can't see your pictures. Can you upload them again in attachment? |
This contribution was helpful to
1 thankful Users |
Follow us on