11/15/2021 11:35 AM | |
Joined: 10/11/2021 Last visit: 4/4/2022 Posts: 2 Rating:
|
Hi, I tried to use PLCSIM (not advanced) together with WinCC Unified, but it is not working. I can download to PLCSIM and to WinCC Unified, but there is no connection. Is it possible I need to change/ set something in the PG/PC Interface like u need to do when u use PLCSIM advanced? Or is there another problem? I hope you can help me. Thor Luyten ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2021 14:04:10New subject after splitting |
|
11/15/2021 2:40 PM | |
Joined: 2/17/2020 Last visit: 9/11/2025 Posts: 1251 Rating:
|
Hi ThLu, I'm afraid this communication between standard PLCSIM and simulated Unified Panel is only possible as of TIA V17. SIMATIC STEP 7 incl. Safety, S7-PLCSIM and WinCC V17 TRIAL Download |
A rating will be well appreciated. |
|
11/15/2021 4:26 PM | |
Joined: 2/17/2020 Last visit: 9/11/2025 Posts: 1251 Rating:
|
Hi ThLu, Okay, in that case I recommend you follow the Pegaia directions in the next post. In addition, please verify that the PG-PC Interface is correctly configured. |
A rating will be well appreciated. |
|
7/12/2022 4:08 PM | |
Joined: 2/4/2019 Last visit: 4/18/2025 Posts: 5 Rating:
|
Hello itafusna, I am also stuck on this point, on what parameter should the PG/PC be set? Thank you for your help.
|
1/6/2023 11:21 AM | |
Joined: 11/28/2022 Last visit: 8/19/2024 Posts: 18 Rating:
|
Did you get this fixed? Did you check Pegaia directions? |
Last edited by: Zed1 at: 01/06/2023 11:23:10 |
|
Follow us on