12/2/2021 11:55 AM | |
Joined: 3/26/2018 Last visit: 8/28/2025 Posts: 3 Rating:
|
Oh, yes. Forgot to mention. It is Version 17 Update 1 on Windows 10.0.19043 |
12/7/2021 10:41 AM | |
Joined: 3/3/2021 Last visit: 11/12/2024 Posts: 271 Rating:
|
Hello AutoGen, maybe Siemens Support can also help with this Topic, I would give it a try. Best Regards, Fred |
4/11/2022 1:33 PM | |
Joined: 11/23/2016 Last visit: 10/16/2024 Posts: 9 Rating:
|
Hi I was also having this issue with "Partly running" and not having connection to the PLC from the simulated WinCC Unified panel. I ended up with support guiding me through the changes I had to make on my computer and I thought I'd share it here, as this was the forum post that got me the closest without actually solving it. The support guy shared a link on the solution and a pdf about the certificate handling. Manual, Entry ID: 109798671 - Look in the last 2 sections "Certificate configuration..." and "Simulation with S7-PLCSIM" Maybe this could be of help to someone in the future. Btw. my VM is a OEM running 21H2 AttachmentCreateCertificatesV17Up2_11Feb22.pdf (2094 Downloads) |
This contribution was helpful to
3 thankful Users |
Follow us on