3/21/2025 8:24 AM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi Evgen_bond, Unfortunately as WinCC Unified and WinCC Professional are two separate systems, there is not simile way to migrate them You would need to re-engineer the system. Unfortunately I have not performed a migration as such but I can tell you (in answer to questions 2 and 5) that there is currently no documentation and no program available to perform the migration. About the other questions I could not tell you but surely it would be necessary to reconfigure everything from scratch since both platforms work in different ways. I hope someone can shed more light on the other questions you ask. Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on