8/18/2025 12:39 PM | |
Joined: 1/21/2013 Last visit: 9/10/2025 Posts: 4101 Rating:
|
Hi Fawzi, In my opinion, the described behaviour indicates that you do not have the WinCC Unified PC Runtime V20 - UPD 2 version installed, which is necessary in order to use the V20.0.0.2 device version. Kind regards |
This contribution was helpful to
1 thankful Users |
9/3/2025 11:00 AM | |
Joined: 8/3/2009 Last visit: 9/10/2025 Posts: 16380 Rating:
|
Hello mfawzi89 Yes I know what Stefan means... I think the same. In your description in the screenshot we only can see that you have selected the Device Version V20.0.0.2 but you do not have mentioned that you have installed the Upd2 for the PC RT/simulation If you simulate you use the Unified PC Runtime software. This is not updated with the common TIA Portal Update -> Check if you have installed this one: https://support.industry.siemens.com/cs/de/en/view/109963700 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on