Industry Online Support
Technical Forum
10/31/2008 10:09 AM | |
Joined: 3/21/2006 Last visit: 10/1/2024 Posts: 10229 Rating: (1181) |
Hello You can find information in this tread: DESIGO information (thanks to Mr. dchartier ) regards |
10/31/2008 2:49 PM | |
Joined: 9/27/2006 Last visit: 10/1/2024 Posts: 12283 Rating: (2685) |
Hello guys; I didnot have occasion to use OPC between OInsight and S7 CPUs, but here it is stated that Desigo Insight-OPEN will use Simatic Net OPC client over Profibus or Industrial Ethernet to connect to S7 PLCs: http://www.siemens.nl/sbt/doc/klt/N9756en.pdf Working with Desigo units was a good experience, but I've always been frustrated that there was no easy way to use industrial-grade Siemens modules for my plants. This is not to denigrate the SBT unit, but I'm used to S7 CPUs and would like to continue working in the same environment , using the same softwares... Maybe I'm getting old. Recently I came across this information, maybe others would like a look at it also. SBT has released (only in Germany for the moment) an HVAC library for S7-300 and S7-400 CPUs. They call it HVAC-Easy Select, and can be programmed in LAD, FBD and STL, using the Step7 environment. http://pcs.khe.siemens.com/index_simatic_hvac_easy_select-6759.htm I have also found that the licensing process for these library products is slightly different that our usual way: the license is integrated in the MMC (S7-300 CPUs) or in the EPROM (S7-400 CPUs) and is locked to a single unique CPU. It cannot be transfered to another CPU, not even for development purposes in-house. That will take some adjustments... I wonder if anyone from the german forum could find oput if anyone there has had any experience with these libraries, just to see how efficient and esay to usethey are. Regards, Daniel Chartier |
Last edited by: dchartier at: 10/31/2008 5:32 PM |
|
11/3/2008 3:40 PM | |
Posts: 65 Rating: (1) |
Thanks for the info. The last part whit the part of using standard cpu and SIMATIC HVAC Easy Select looked good, looking forward too see what it looks like. |
Follow us on