4/18/2022 10:47 AM | |
Posts: 3 Rating: (0) |
Hi Guys, New to this forum. Recently, we have encountered a problem with our WINCC explorer. When starting the wincc project and clicking play, it loads the program for a long time and them prompts a message "AN ERROR HAS OCCURED THAT REQUIRES A RESTART OF THE COMPUTER" CLOSE ALL APPLICATION IF POSSIBLE, AND TRIGGER A RESTART WITH THE OK BUTTON. I have also attached the picture for you to view. The system was shutdown for a long time and we would like to run the system again however this error occurs everytime we open the project and or during auto-play. I'm not sure what is the problem. The connection to the PLC is ok. I think this is related to the project and might need to check something on it but I'm not an expert. Hopefully you could help us. Thank you AttachmentDoc1.docx (280 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on