4/16/2022 11:17 AM | |
Joined: 4/16/2022 Last visit: 4/20/2022 Posts: 1 Rating: (0) |
I have the following issue While configuring S71500 PLC in TIA Section Tool: Limit->>> Current Consumption Current Consumption Rated Value: 2.8A (with hazard symbol) Current Consumption Peak Value: 2.7A (with hazard symbol) Two separate External Power supplies are considered for both PLC & DO modules. Please find the attached PLC configuration details for reference. AttachmentCONFIGURATION ERROR.pdf (536 Downloads) |
Follow us on