12/12/2023 10:56 AM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33783 Rating: (4195)
|
I'm sorry, but I don't understand your functional description. |
12/12/2023 11:09 AM | |
Joined: 11/30/2021 Last visit: 9/12/2024 Posts: 17 Rating: (0) |
Hi, Sorry I forgot to upload my program. So my version works only when timer B002 is set to two seconds.When I put more than two, the outputs starts to be activated at the same time. That's, because I don't know how to make timers dependant on each other. AttachmentProgram_2.zip (395 Downloads) |
Last edited by: FST MUL at: 12/12/2023 11:11:31 |
|
12/12/2023 11:15 AM | |
Joined: 4/14/2018 Last visit: 9/18/2024 Posts: 46 Rating: (1) |
When asking help please provide details like PLC model and Software name and version used. |
|
|
12/12/2023 11:17 AM | |
Joined: 11/30/2021 Last visit: 9/12/2024 Posts: 17 Rating: (0) |
Hi, Sorry, here it is: Logo!Soft Comfort v 8.3 and Siemens LOGO! 6ED1052-1CC08-0BA1 EDIT! I will also try to explain the machine a little bit. So it is a rubber material cutter. There is a roll of material ( picture rolled up paper) and it is rotated by electrical motor (B002). When the material is came of the roll enough. B002 stops and the blade (B004) will cut the material. This is fixed time and is operated by single way pneumatic cylinder. And after that, the air (B006) blows material if it has gotten stuck. This is also fixed time. Also there is counter, how many cuts have to be done. I know there is a probably too many redundant steps in the program, but I don't know any better. EDIT2! Okay so I made it. I had way too much extra stuff there. I uploaded the version, maybe someone have time to check if this can be made even more smaller and simpler. AttachmentProgram2.zip (290 Downloads) |
Last edited by: FST MUL at: 12/12/2023 12:30:04Last edited by: FST MUL at: 12/12/2023 12:31:00Last edited by: FST MUL at: 12/14/2023 14:41:46 |
|
Follow us on